This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5755M: SSTIMER should be disabled in case 2.1ch?

Part Number: TAS5755M

Hello

My customer intend to use 2.1ch for TAS5755M .

I had tested TAS5755MEVM by myself.

SSTIMER pin is as default ( 2.2nF is between SS timer and gnd)

In case 0x1A register is 1Ah ( SSTIMER enabled), POP is seen, 0x1A is 88h, no pop.seen.

( see attached )

 

Is my test correct?

SSTIMER function should be disabled in case 2.1ch? ( Is customer should so, pop in case 2.1ch is same level

as 2ch BTL?)

 

Please advise

Best Regards

 

TAS5755_SE_POP_EVM testing.pptx