Hi Team,
One of my customer is using LMK04208 for ZCU111 Xilinx RFSoC. The output Clock frequencies required is as below.
- OUT0 -> 7.68 MHz
- OUT1 -> 7.68 MHz
- OUT2 -> 245.76 MHz
- OUT3 -> 491.52 MHz
- OUT4 -> 491.52 MHz
The inputs:
CLKIN0 -> 122.88 MHz
CLKIN1 -> terminated in connector
Customer requirement is: Feed 10MHz to CLKIN1. Do not use CLKIN0.
Customer have arrived on the values for the configuration they require. Can you please review/validate the attached configuration?
Regards, Shinu Mathew.