Hello:
I met some problems I can't sovle.
I use the Tics pro software to generate the register data as the above pictures showed,then I export the register data to a txt file. Then I use the SPI port to transfer the data to LMK04832 in order showed in txt file.I am sure the data is correctly configured to LMK04832,because I can read the LMK04832 register data from the SPI port and the reading data is what I transfer to it.But to my surprise, the LMK04832 can't work,some channels have no clock out and some channels have the wrong clocks,for example,13.5MHz clock. No matter how I change the N divider number or other number, the result is the same. So I really don't know what to do next and where I am wrong, I sincerely hope your help, thank you!