This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Intent to drive CDCLVP111 with a +1.8V LVCMOS oscillator. The question is if the negative input of CDCLVP111 is set to 0.9V (1.8V/2) as the threshold voltage and the oscillator is connected to the positive input, is it violating the required minimum Vcm voltage of 1V?
Hello Chong Kim,
I will let Jennifer comment on this.
Best,
Aaron Black
Hi Chong,
What is the oscillator part number and what are your VIH/VIL values? This information is needed for me to determine if the VCM is violated.
Regards,
Jennifer
Chong,
The recommended supply voltage is 2.5V or 3.3V. Are you using 1.8V as your supply?
Regards,
Jennifer
Hello Chong Kim,
The Vcm should be set based on CDCLVP111 Vcc not Oscillator Vcc. If you are trying to utilize 0.9V (1.8V/2) of Vcm this does not meet requirements.
The 0.9V is for Vth, not for Vcm. The question was how to interface a +1.8V LVCMOS signal to CDCLVP111? Aside from setting Vth = 0.9V, are there any other issues that need to concerned with? Does Vcm even matter for interfacing a LVCMOS signal to CDCLVP111?
Hi Chong,
The VCM must be within the specified datasheet range when the inputs are DC coupled. You'd have to change the external biasing circuitry to match the datasheet requirements. If the inputs are AC coupled, then the VCM does not matter.
Regards,
Jennifer
Hi Chong,
VTH needs to be at least 1V to meet part requirements. Using 0.9V would not appropriate for your design.
Regards,
Jennifer