Hi, Datasheet says register address 0x117, field DCLKoutX_FMT---LVPECL 1600mV and LVPECL. What is the difference between the two? I am trying reducing the output swing from LMK for LVPECL outputs. Thanks, Abhijit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Datasheet says register address 0x117, field DCLKoutX_FMT---LVPECL 1600mV and LVPECL. What is the difference between the two? I am trying reducing the output swing from LMK for LVPECL outputs. Thanks, Abhijit
Hi Abhijit,
The datasheet specifies the following:
LVPECL can be either have a 1600mV or 2000mV output peak to peak swing. i.e. field value = 5 would have the lowest swing.
Regards,
Jennifer
Hi, What is the output voltage swing for Field value 0x07 (LCPECL)? thanks, Abhijit