Konrad
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Konrad,
In this case, it is not obvious what the cause is, but here's two experiments that likely will be able to direct us towards the root cause.
1. Theory #1: Cycle Slipping
- CSR doesn't help, so I don't think cycle slipping is the issue. But you might want to also try to change the charge pump current to change the loop badnwidth without changing the phase detector frequency and not N divider or phase detector frequency. If you have it maxed out, try reducing this current and seeing if it agitates the problem. I expect it not to, but if it does, then reconsider cycle slipping.
2. Theory #2: N Divider
If there is some issue related to the N divider, try reducing the modulator order or the PFD_DLY settings to see if it has an impact.
3. Theory #3: Misprogramming
Just want to make sure that there is no programming issues causing this.
4. Theory #4: Input reference
The input doubler works by clocking on both the rising and falling edges of OSCIN. If there is an issue with OSCin, such as it NOT having 50% duty cycle, then this would cause very high jitter, maybe enought to cause locking issues. To test this theory, try driving with a signal generator.
Also, one diagnostic to try would be to try direct 200 MHz from a signal generator without the doubler to help discren if the issue is related to the N divider or the doubler.
Regards,
Dean
Hi Dean,
narrowing down from the points that you've mentioned, I've focused my attention back to cycle slipping, which in fact turned out to be the problem.
In my previous measurements FL_TOC value was set too low.
Eventually for (FL_TOC = 200 and FL_CSR = 2x) I was able to jump in practically entire VCO range (9.4~10 GHz) with no lock problems.
Thanks for help,
Konrad