Hello Sir,
I'm Using LMK01801, out of these dividers CG1 to CG4, CG2 only working in my board, I've set all Clocks in LVDS mode, Please help us.
Thanks & Regards,
Venkatesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Venkatesh,
Can you please share your register programming, or potentially your TICS Pro .tcs save file if you're using TICS Pro?
Regards,
Derek Payne
Dear Sir,
Please find the attached .tcs file,
Test/CLKoutTYPE_0 is Connected to ground with a resistor of 1Kohm.
SYNC0/CLKoutTYPE_1 is Connected to ground with a resistor of 1Kohm.
SYNC1/CLKoutTYPE_2 is Connected to ground with a resistor of 1Kohm.
we are not using SPI mode, we have fixed hardware, and also what happen if we connect (bias-pin no-26) to +3.3V
Thanks
Hi Venkatesh,
Also, I suspect the common mode voltage could be affected if bias is directly connect to 3.3V, but I don't think that would cause the dividers to stop working. We recommend connecting a 1uF cap between the bias and Vbias pin.
Regards,
Jennifer