Part Number: LMK05028
Hi team,
When using 2-Loop REF-DPLL Mode without TCXO, how much frequency stability can be achieved? Customer hopes +/-15 ppm.
What other parameters does affect frequency stability in LMK05028?
Best regards,
Hideki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK05028
Hi team,
When using 2-Loop REF-DPLL Mode without TCXO, how much frequency stability can be achieved? Customer hopes +/-15 ppm.
What other parameters does affect frequency stability in LMK05028?
Best regards,
Hideki
Hideki-san,
if the DPLL is locked to the reference, the accuracy is determined by the input.
If the DPLL is in hold over or free running, the XO will be the limiting factor. In order to achieve +/- 15ppm the XO need to be equal or better then this.
Regards,
Julian