This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Further to my original question “LMK05028: Problem getting PLL2 to both phase and frequency lock to IN0 ref input” on 29-Oct-24, I now have another problem. PLL2 is configured in 2-loop REF-DPLL mode.
I want to use the 4 reference inputs for PLL2 and have started my tests using the LMK05028 evaluation board, using the DIP switches to change the ref input selection.
IN0 is connected to an output from PLL1 running at 156.25 MHz. PLL2 locks correctly to this reference clock.
IN1 input is configured to lock to a frequency of 62.5 MHz. If I generate this frequency using PLL1 and connect it to IN1 input, PLL2 locks correctly. However, if I connect this to an external source (another board of our design or a frequency generator), then PLL2 will not lock (APLL2 generates the correct frequency, but REF-DPLL2 will not frequency or phase lock).
We have the LMK05028 device on a board of our design. I have essentially the same PLL configuration programmed onto two of these boards, the two boards being connected together using optical fibre. One of the boards uses the output from PLL1 to drive an SFP module. The second board recovers the clock from its SFP module (62.5 MHz) and inputs this as a reference to IN1 of PLL2. The idea being that I can then run the processing on the second board using a 156.25 MHz clock which is locked to the 62.5 MHz recovered clock.
In my test setup using two boards I get the same results as when using the evaluation board. I can get PLL2 to lock if I provide it with a reference from it local PLL1. However, as soon as I source the recovered clock from the other board, then PLL2 will no longer lock.
I currently have the input monitors disabled. Are these only used to generate the various lock flags or do these have an impact on the operation of the PLL as well?
Do the DPLL Frequency/Phase lock detectors only affect the lock flags or do they impact the PLL operation as well?
Unfortunately, I only have one evaluation board otherwise I could try a setup with two boards linked to each other.
Best regards,
Gary
Hello Gary,
The input monitor does affect how the PLL operates.
If you were to disable the input monitor detector the DPLL may lock to noise and not just the intended frequency.
The DPLL Frequency/Phase lock detector is just for status and will not affect the device. But I would suggest leaving them enabled.
I will begin testing to see if I get a similar issue.
Best Regards,
Kyle Yamabe
Hello Gary,
Since the two boards are using the same configuration the output format for the 62.5MHz clock is CMOS but the input format for IN1 is DC-DIFF. Changing the input type on IN1 to LVCMOS may fix your issue if the output type is not correct it could cause the device to read different frequencies which could prevent locking.
Best Regards,
Kyle Yamabe