Part Number: LMK05028
Tool/software:
I am trying to use the LMK05028 part to generate a reference clock using PLL1 and clean an incoming clock using PLL2.
I am using the evaluation board, where the XO frequency is 10 MHz and the TCXO frequency is 48.0048 MHz.
All clock outputs are 156.25 MHz. For my test setup I have connected OUT6_P (sourced from PLL1) to IN0_P (configured as CMOS and LVCMOS, respectively). I have configured PLL1 in 2-loop, TCXO-DPLL mode which just free-runs. I have configured PLL2 in 3-loop mode and want to use the REF-DPLL to lock to an incoming reference clock that is input on IN0.
The current situation is that both PLLs lock and produce 156.25 MHz clocks on all outputs. However, the problem I have is that PLL2 is neither phase nor frequency locked (LOPL_DPLL2 and LOFL_DPLL2 are both set). From this I imagine that the TCXO-DPLLs and APLL2 are both locked, but REF_DPLL2 isn't. The status information indicates that reference IN0 is being used and if I unplug this input the status changes and I believe PLL2 then free-runs.
I have tried lots of different settings without any improvement. Therefore, I am after some help with this please.
I have attached the TICS Pro .tcs file with the configuration that I am currently using.