Part Number: LMK5C33216
Hello,
There are two ROM startup conditions that are available.
However, these both assume a 10 MHz at IN1 and XO= 38.88 MHz. What are the outputs doing if IN1 is unconnected and XO input is 100 MHz? What output frequencies are generated?
Also, I noticed that in TICS Pro 1.7.4.0 the APLL settings/vco frequencies seem to not load correctly from a .tcs file created in version 1.7.3.0. Where can I get a copy of the version 1.7.3.0 software.
Thanks,
Jon