Part Number: LMK05028
Other Parts Discussed in Thread: LMK05318
Hi all
Would you mind if we ask LMK05028?
<Question1>
How much of value should we set these value?
-Frequency Detect Threshold
-DPLL Frequency Lock Detectors
-DPLL Phase Lock Detectors
-XO input tolerance : ±25ppm
-Reference input tolerance : ±30ppm
<Question2>
Is it to possible to operate following reset in a row?
Register R12 : Software Reset ALL functions
Register R676 : Software Reset Output Channels
Register R677 : Software Reset PLL2 , Software Reset PLL1
As the background of this question, the customer operates "Register R12 : Software Reset ALL functions" in a row", the output clock was not unstable.
Kind regards,
Hirotaka Matsumoto