We are using the following register set to configure the LMX2571:
R60 0x3C0000 R58 0x3A0000 R53 0x350000 R47 0x2F6000 R46 0x2E0000 R42 0x2A0000 R41 0x290007 R40 0x280780 R39 0x270000 R35 0x230000 R34 0x220000 R33 0x210000 R32 0x200000 R31 0x1F0000 R30 0x1E0000 R29 0x1D0000 R28 0x1C0000 R27 0x1B0000 R26 0x1A0000 R25 0x190000 R24 0x180000 R23 0x170000 R22 0x160000 R21 0x150000 R20 0x140000 R19 0x130000 R18 0x120000 R17 0x110000 R16 0x100000 R15 0x0F0000 R14 0x0E0000 R13 0x0D0000 R12 0x0C0000 R11 0x0B0000 R10 0x0A0000 R9 0x090000 R8 0x08000E R7 0x070EC4 R6 0x060606 R5 0x050101 R4 0x041014 R3 0x030000 R2 0x02978D R1 0x01009E R0 0x000001
On the demodulated output we do not get any meaningful signal. Can you please verify whether this configuration is correct? We used the "TICS Pro"-Tool to generate that configuration, but we are working on a custom hardware.