Hello,
First, I work with integer mode with LMX2594 and two external generators, both locked on 10Mhz lab reference.
Lab Gen1 =Fosc=128Mhz; FreqPFD=32 Mhz ; LMX2594 Fout = 7744Mhz
Lab Gen2 = 7744Mhz+128Mhz=7872Mhz
Un mix both previous signals with RF mixer: I keep de 128Mhz différence to oscilloscope
I look also the Gen1 signal to osciloscope
Thus I can see the phase between both 128 Mhz signal with oscilloscope : No phase drift , I adjust the phase difference to 0° ( Lab Gen phase adjustment), all devices are phase locked, all is ok
I simulate the loose of Fosc signal, thus I switch RF on:off (front panel generator, or coax removed)
When Fosc is ‘’on’’, LMX2594 lock again. But… phase difference could be 0° or 180° : random
Could you provide more information about phase detector curve response? Is it 0-2PI or 0-4PI or.. ?
I don’t have the same behavior with other integer PLL system: phase is always the same.
See attached tcs file
Regards7744integermode.tcs