hi TI,
Question 1
The datasheet of LMK1d1208 writes the input 50% duty cycle clock, and the output duty cycle is 45%-55%. If the input clock duty cycle is 2% (200kHz), what is the output duty cycle float?
Question 2
Can LMK1d1208 be used as LVDS data transmission?
Question 3
The input signal is a 200kHz LVDS signal with a duty cycle of 0.2%-0.6%, and outputs more than 6 channels of the same LVDS signal. The temperature range is -40-105 degrees. It is best that each channel can have a separate enable signal. Can you recommend a chip that meets the above requirements?