This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: Recommended pin condition during power up

Part Number: CDCE62005

Hello team,

Could you let me know if there is any requirement on below pins during power up? for example, it needs to be pulled to GND, floating is fine, and so on.

  •  AUX_IN
  • PRI_REF+/-
  • SEC_REF+/-
  • SPI_CLK
  • SPI_LE
  • SPI_MOSI
  • SPI_MISO

Best regards

  • Hi Taketo, 

    Aux is for xtal input only. Can be left floating if not used. 

    Pri_Ref & Sec_Ref, depending on which input you use, connect it with a 1k Ohm resistor to GND. 

    All the SPI pins can be left floating, will default to logic level 1. 

    Regards, 

    Vicente