Other Parts Discussed in Thread: TPL5110
Hi team,
Equation of the Tadc is different between TPL5110 and TPL5110-Q1.
Which is the correct equation?
I would like to select time interval = 2.6s.
Tadc from equation (3) in TPL5110 gives
Tadc=2
While equation (4) in TPL5110-Q1 gives
Tadc = 5
If my understanding is correct, this device can not select time interval between 2s and 3s?
regards,