Part Number: LMX1204EVM
Other Parts Discussed in Thread: LMX1204
Hi,
I have difficulties using the LMX1204EVM in diviser or multiplier mode. Buffer mode work as intended but diviser and multiplier mode output the same spectrum as buffer mode.
For example in divide by 2 mode, with a 6 GHz input frequency at 3 dBm, output spectrum is the same than in buffer mode even after applying a reset (see screenshot and registers below).
I'm using v.1.7.5.7 of TICS Pro.
Did I miss a parameter to config ?
Thanks in advance,
Samuel
R90 0x5A0000 R86 0x560000 R79 0x4F0000 R75 0x4B0000 R72 0x480000 R67 0x430000 R65 0x410000 R34 0x220000 R33 0x210000 R29 0x1D0000 R28 0x1C0000 R25 0x19000A R24 0x180001 R23 0x172040 R22 0x160800 R21 0x150000 R20 0x140000 R19 0x130000 R18 0x120000 R17 0x110000 R16 0x100000 R15 0x0F0800 R14 0x0E0000 R13 0x0D0003 R12 0x0C0000 R11 0x0B0000 R9 0x090000 R8 0x080010 R7 0x070000 R6 0x060000 R5 0x050000 R4 0x040000 R3 0x034007 R2 0x020100 R0 0x000000