The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04031: Audio Need to generate 1x 2x 4x of 45.1584MHz & 49.152MHz Very low jitter.

Part Number: LMK04031
Other Parts Discussed in Thread: LMK5B12204, LMK04821, LMK04832, LMK6C, LMK6P, LMK00804B

Hi Experts,

Good day.

Our customer needs to generate 1x, 2x, and 4x multiples of Audio frequencies 45.1584MHz & 49.152MHz on a single output, multiple of which can be selected by software or inputs with extremely low jitter ~100-200fs. They need to reclock Audio SPDIF/ADAT/I2S signals. And found your LMK04031BISQ as an example. Using your Clock Design Tool, they are not able to set it up using the wizard.

Is this something they could do with that LMK04031BISQ chip? If not, any other chip? If yes, any help?

Thank you very much

Regards,

Josel

  • Hello Josel,

    Why did you pick LMK04831? When I ran the Clock Design Architect based on your requests, it did not suggest the LMK04831 as a solution. Apart from programming one output to different frequencies and having ~100 to 200 fs of jitter, are there any other features that you need? Do you have a set input frequency? Any specific output and input types (i.e LVPECL, LVCMOS, LVDS)? Also, do you require 2 different outputs, outputting the different family of frequencies, or two separate devices?

    Note that our LMHxxxx devices are made for audio applications, but it seems that the jitter from those devices won't fit your requirements. Here in blue you can take a look at them in case they do meet them and the customer is not as stringent on jitter.

    Thanks,

    Andrea

  • Hi Andrea,

    Good day.

    Thank you for your very good questions!
    On Input, I need 2 clocks 45.1584MHz & 49.152MHz.
    On Outputs, I need more than 1 yes
    1]One that goes to the reclock (COAX/Optical/I2S), using a differential clock I can find a very low jitter flip flop.
    2]One that goes back to the CPU (actually an XMOS) to get the bits generated at the right time (not differential)
    3]I may need more than 1 for point 1 above as I have not yet found a solution to reclock I2S staying very low in jitter.

    On Outputs, better to have differential output as mentioned above because low jitter flip flops use differential which makes sense.

    For inputs, can I have only one clock and generate all multiples 1x/2x/4x for both base clock frequencies with the right precision? I was thinking having the 2 clocks dedicated would be better, I can find clocks at above 50fs if needed (crystech and accusilicon).

    Hope I answered your questions and better explained my need.

    Thank you very much!

    Regards,

    Josel

  • Hello Josel,

    One last clarification question, when you say:

    For inputs, can I have only one clock and generate all multiples 1x/2x/4x for both base clock frequencies with the right precision? I was thinking having the 2 clocks dedicated would be better, I can find clocks at above 50fs if needed (crystech and accusilicon).

    Are you looking to have one input or two inputs and you switch between them? From what you said above I believe you contradicted yourself.

    If possible, could you also provide a visual/diagram demonstrating your need. I am still not fully understanding your description and want to make sure I design the correct solution for you. Thanks!

    Best,

    Andrea

  • Hi Andrea,

    LMK5B12204 might be better adapted? Does TI have a low jitter multiplexer (2:1)?

    Regards,

    Josel

  • Hi Andrea,

    Because audio requires quite precise frequencies, I was thinking to use 2 input clocks with frequencies of 45.1584MHz & 49.152MHz (which can be doubled if needed), you can check here www.audiophonics.fr/.../composants-electronique-horloges-c-600.html to better understand.

    Then I need, from the control bus (I2C preferred BTW), to programmatically select between the 2 inputs and the multiplier 1/2/4x depending on the type of audio file being read.

    But if you think, because of the TI chip capabilities, I can only use one input at the frequencies TBD and generates the above frequencies and their 1/2/4x multiples, I am open to any suggestions.

    Hope this is clearer, thanks for your support!

    Regards,

    Josel

  • Hello Josel,

    I'll get back to you by the end of the week

    Best,

    Andrea

  • Hi Andrea,

    Good day,

    Actually, I may just only need the 2:1 multiplexer. What could you recommend as a very low-jitter 2:1 multiplexer? If you have a D flip flop too let me know.

    Regards,

    Josel

  • Hello Josel,

    Thank you for the update, I'll reply with a recommendation by tomorrow.

    Best,

    Andrea

  • Hello Josel,

    From my understanding you need a device that:

    Has 2 inputs that can be:

    1) switched between them through I2C

    2) multiplied after being inputted.

    Has 2 outputs:

    1) First output needs to be low jitter (around ~100-200 fs) and differential with frequency unknown as of right now

    2) Second output should be single-ended with it's frequency unknown

    If I have understood your use case, then note that I cannot give you an optimal recommendation with the output frequencies you are trying to use. For your user application I would recommend the LMK3806B. The LMK04821 and LMK04832 would also work and would result in lower jitter than the LMK3806B, but may be more complicated to use. The LMK5B12204 that you suggested may not work since it may not output the frequencies you desire (if you just want to output your input) and it will be more complicated to use than the other suggestions I gave. Again, I can give you better support if you tell me your output frequencies and if you can include a block diagram that would be extremely helpful. Thanks!

    Best,

    Andrea

  • Hi Andrea,

    Good day.

    Thank you but I need 2 inputs.
    Here is the block diagram.


    Please advise.

    Regards,

    Josel

  • Hi Andrea,

    Good day.

    I decided to go with 2 crystech clocks, a Low Jitter Clock Buffer/MUX, flip flop. And for I2S, I will use a Sample Rate converter (you have some BTW).

    Regards,

    Josel

  • Hello Joselito,

    If you require two inputs that are processed at the same time, then you are correct, you need to separate oscillators. I understand you have chosen to go with Crystek, but we also offer stand alone oscillators that can produce frequencies higher than 50 MHz, the LMK6P for a differential LVPECL output and the LMK6C for a single-ended LVCMOS output.

    We also have several buffers that can fan-out 2,3, or 4 frequencies either differential or single-ended such as LMK00804B. You can find more options in this link, but do note that some options listed can only do single-ended or differential outputs and not both.

    Glad you could use one of our sample rate converters!

    Best,

    Andrea