Part Number: TLC555
Other Parts Discussed in Thread: LM555,
Good Day,
As part of a project I have implemented a circuit using a 555 timer to capacitively pick up spark plug impulses from a petrol engine. The purpose of this circuit is to convert a spark plug impulse and turn it into a square wave that can be read by a microcontroller. The circuit was initially implemented using a LM555 timer running at 3.3v. The below images show the input waveform (blue) from the engine spark plug, and the output from the 555 timer (yellow).


The layout of the circuit as as shown below:
Once proof of concept was achieved using the DIP package, I selected the TLC555 timer to replace the DIP package for a surface mount design. However, it appears that this IC does not produce the same results as the LM555 at 3.3v. The TLC555 either remains at 0v, or triggers intermittently until an operating voltage of 5v is reached. I would very much appreciate some assistance in either finding a part that has an equivalent performance to the LM555 or some tips for troubleshooting the problematic behaviour with the TLC555.
Below are some images of the initial testing, followed by an image of the non-functioning TLC555 circuit.

Thank you,
Regard,
Bjorn