Part Number: TLC555
Tool/software:
Hi team,
My customer wants to build a serial time delay structure. And totally based on the example schematic of our datasheet, but only with the first two TLC555.

They found that:
1. The first TLC555 sends a pulse, and a 1nF capacitor needs to be added to the input port
2. The first TLC555 needs a certain time interval for the input of the TRIG signal to send a pulse. After testing, it is found that the first tlc555 thres has been discharged, and the input capacitor has also been discharged. What parameters determine this time interval and how to calculate it?
3. For the TLC555 to output a pulse normally, it must be a signal pulse from low to high. The input signal cannot be low or high all the time.
Could you please help to answer these questions?
Thanks!