Hi Team,
Customer have a few question for TPL5110-Q1
1. If only timing wake-up feature is used, Are they supposed to pull down corresponding voltage on DELAY/M_DRV PIN pin?
2. In the early stage of design, customer wanted to use MCU to control M_DRV_DOH and designed as per datasheet to control MOS.
But in the end they do not want to use this feature, so customer would like to know if it is possible to cancel/remove M_DRV_DOH signal.
3. In datasheet it mentioned that DELAY/M_DRV is briefly pulled VDD, what is the purpose/function of manually turning on the MOS?
To reset counter? if this is the case then is it the same as controlling VDD to disconnect RST_TIMER_DOH?
Thanks