Part Number: CDCE6214
hello,
My schematic is designed to use a 25MHz crystal as ref clk, after configuration, we can view 25MHz wavefrom from the crystal pins. but the pll can't lock, so I config Y0 as output and source from refclk. but there is no any signal on CDCE6214 pin7. We also tried to config Y1 source from refclk and still get nothing. so how to debug the hardware? is the amplitude of crystal too small? the oscilloscope shows that the peak-peak voltage is about 1.5V,I thing the amplitude is enough, but why I still can not get the refclk?