Dear Team,
One question about CDCI6214.
Could you provide slew rate result of LVDS output?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jimmy,
The slew rate is not directly provided, but the differential output voltage and the rise/fall time are both provided in the datasheet. With both of these values, the slew rate can be calculated.
Taking the typical values listed in the datasheet (noting that the time is 20% to 80%, or 60% of the total swing voltage), this would be 0.267 V/ns.
Thanks,
Kadeem