Other Parts Discussed in Thread: LMK6C
Hi,
I need your expert advice.
The idea is to use this component as basic LVDS output OSC with 3 outputs 250, 50 and 100MHz
1. I can not use pins 43 (Auxin), SECREF(3,2), and PRIREF(45,46) in order to provide 250, 50 and 100MHz outputs only to TI DSP 6655?
2. If I am not using the PRIREF should I connect these pins as unused SECREF?
3. Also, can I not use the EXT_LF(P/N) (pins 40,41)? if no, leave them floating or PD/PU?