Hi Team,
I'm using TB_FMCH_DP3 Board and lmk04906 is monunted on TB_FMCH_DP3.
And i want to generate 135M clock(from clkout0 port) to supply reference clock from lmk04906 to gty(gigabit transceiver) on Xilinx VCU118 Board.
And TB_FHCM_DP3 hardware document guide register setting value of 135M clock from clkout0 like below
R 0(0x00000012) - 0x00000240 (0000_0000_0000_0000_0000_0010_0100_0000)
R 1(0x00000012) - 0x00000241 (0000_0000_0000_0000_0000_0010_0100_0001)
R 2(0x00000012) - 0x00000242 (0000_0000_0000_0000_0000_0010_0100_0010)
R 3(0x04000001) - 0x80000023 (1000_0000_0000_0000_0000_0000_0010_0011)
R 4(0x04000000) - 0x80000004 (1000_0000_0000_0000_0000_0000_0000_0100)
R 5(0x04000000) - 0x80000005 (1000_0000_0000_0000_0000_0000_0000_0101)
R 6(0x00888000) - 0x11100006 (0001_0001_0001_0000_0000_0000_0000_0110)
R 7(0x00888000) - 0x11100007 (0001_0001_0001_0000_0000_0000_0000_0111)
R 8(0x00888000) - 0x11100008 (0001_0001_0001_0000_0000_0000_0000_1000)
R 9(0x02aaaaaa) - 0x55555549 (0101_0101_0101_0101_0101_0101_0100_1001)
R10(0x008a0200) - 0x1140400a (0001_0001_0100_0000_0100_0000_0000_1010)
R11(0x002c0881) - 0x0581102b (0000_0101_1000_0001_0001_0000_0010_1011)
R12(0x00d8600b) - 0x1b0c016c (0001_1011_0000_1100_0000_0001_0110_1100)
R13(0x01d80003) - 0x3b00006d (0011_1011_0000_0000_0000_0000_0110_1101)
R14(0x00918000) - 0x1230000e (0001_0010_0011_0000_0000_0000_0000_1110)
R15(0x00000000) - 0x0000000f (0000_0000_0000_0000_0000_0000_0000_1111)
R16(0x000aa820) - 0x01550410 (0000_0001_0101_0101_0000_0100_0001_0000)
R24(0x00000006) - 0x000000d8 (0000_0000_0000_0000_0000_0000_1101_1000)
R25(0x00080030) - 0x01000619 (0000_0001_0000_0000_0000_0110_0001_1001)
R26(0x007d4000) - 0x0fa8001a (0000_1111_1010_1000_0000_0000_0001_1010)
R27(0x00800002) - 0x1000005b (0001_0000_0000_0000_0000_0000_0101_1011)
R28(0x00008002) - 0x0010005c (0000_0000_0001_0000_0000_0000_0101_1100)
R29(0x0000002d) - 0x000005bd (0000_0000_0000_0000_0000_0101_1011_1101)
R30(0x0010002d) - 0x020005be (0000_0010_0000_0000_0000_0101_1011_1110)
But clkout0 didn't output any clock ..
I analyzed register value but i didn't found special problem.
Could you let me know the root cause ?
Thanks,
Doohan