Hi
I do have a question regarding the different Datasheet Revisions for the LMX2592 (latest greatest is Rev. G).
Does the Datasheet Revision correspond to a HW Revision of the Chip? I.e. are there different HW Revisions of the Chip sold from the Production Start up to now? If there are different HW Revisions that need different default register settings, how can I detect the actual HW Revision of the Chip by SW to perform a correct version handling in SW? I did not see any register that would present a Chip HW Revisioning.
If there are no different HW Revisions of the Chip sold from its Production Start up to now, then how would I have to interpret the different values for default bit settings in some registers with respect to the different Datasheet Revisions?
Some examples for the different Register Layouts in the different Datasheet revisions:
* Register 64: Bit Position 4 (counted from 0) up to Rev. C this bit was part of AJUMP_SIZE. From Rev. F this bit shall be set to 1 as default and does no longer belong to AJUMP_SIZE.
* Register 33: Rev. A default value is 0x4210 and starting from Rev. C the default value is 0x2606
* Register 32: Rev. A default value is 0x4210 and starting from Rev. C the default value is 0x2106
* Register 7: Rev. A default value is 0x20B2 and starting from Rev. C the default value is 0x28B2
Best Regards
Rolf