This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is considering using LMK04832 with ADC32RF55. Could you please answer following questions:
- They are assuming a 2.6GHz output as the ADC sampling clock, but what is the required input frequency? Is it either 0.001-250MHz?
- It is a question regarding the dynamic phase adjustment function. How long does it take for the register to be actually shifted by half a clock after being rewritten via SPI communication?
・I think that it is possible to output a trigger signal from the LMK04832,and could you please tell me the shape of signal waveform? Is it pulse-like?
Thank you for your help.
Regards,
Taito Takemura
Takemura-san,
First, please note that LMK04832 VCO0 maximum frequency guaranteed is 2580MHz; if 2600MHz is required, most devices (but likely not all devices) can achieve this frequency, and the full range of temperature calibration may be reduced for devices that can achieve this frequency (see Allowable Temperature Drift for Continuous Lock section in the datasheet electrical characteristics).
Now, your questions in order:
They are assuming a 2.6GHz output as the ADC sampling clock, but what is the required input frequency? Is it either 0.001-250MHz?
LMK04832 is a PLL, so the input frequency has a large range of potentially acceptable values. The restrictions can be summarized as:
In summary, flexibility in input frequency is provided for cases where it is either required or necessary, but typical use cases don't need a broad input frequency range and can pick a normal value like 100MHz as the reference frequency to PLL2. PLL1 is an option to help if the system reference frequency shares a very small common divisor with the desired VCO frequency, or if the reference noise is not very good. But if the reference has good phase noise performance and is at a good frequency, PLL1 is not needed or recommended.
It is a question regarding the dynamic phase adjustment function. How long does it take for the register to be actually shifted by half a clock after being rewritten via SPI communication?
We do not specify any guaranteed timing characteristics for the half-step adjustment period. On the last data bit clock cycle rising edge of a SPI write transaction, the new data to the SPI registers is latched into register state. An internal state machine clock running at nominal 10MHz ± 30% propagates the change across the SPI domain and into the internal register state machine domain, which takes some single-digit number of state machine clock cycles (varies depending on timing variation between internal state machine clock and SPI clock). Once the half-step register result is propagated into the internal register state machine domain, it should only take one or two VCO cycles for the half-step to engage. So I think, from last data bit clock cycle rising edge of SPI to half-step phase adjustment complete, timing is in the range of (0.3µs to 1µs) + (1 to 2 VCO periods), but there may be other factors of which I am unaware. If a more precise answer is required, or if additional verification is needed, please let us know.
I think that it is possible to output a trigger signal from the LMK04832,and could you please tell me the shape of signal waveform? Is it pulse-like?
The SYSREF outputs can be used to generate one or more pulses with width equal to the 2/(FSYSREF). The pulser synchronously outputs full cycles of the SYSREF divider, so setting the SYSREF divider value controls the pulse width.
Regards,
Derek Payne