Hello Team,
Would like to operate the LMK04828BISQ as an LVPECL driver into a NB7L1008M with as few components in the path as possible. There is a preference to connect them directly as a DC coupled path to minimize "noise". Three paths will be used one at 10 MHz, another at 500 MHz, and the remaining one at 2GHz. Can you assist in describing exactly what is needed to accomplish this?
Regards
Vraj T