The horizontal coordinate of Figure 1 above represents the design frequency, and the vertical coordinate represents the actual frequency output, which is 0.1MHz according to the step from 2011MHz to 2013MHz. The test shows that the actual output is 3MHz step output, but there is no linear output
This is why
I have tested the output power and found that the output power is not regular. Is there any way to control it