This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572LP: input level of OSCin (Single-ended input buffer) of LMX2572LP

Part Number: LMX2572LP

I would like to confirm the input level of OSCin (Single-ended input buffer) of LMX2572LP.
In the catalog, the OSCin input voltage is listed as min: 0.3 to max: 3.6V.
Is it safe to assume that this value is Vp-p from Figure 154?
And if the impedance is 50Ω, is it safe to assume that min:-6.48dBm to max:15.11dBm?

Regards,
Akihiko Yokouchi