Part Number: LMX2820EVM
Hello.
I am curious whether the time from SPI CSB to Lock Detect can be within 50us when initially setting the PLL frequency to 12GHz with the LMX2820EVM board and sweeping (up or down) in 0.5Mhz increments.
48MHz will be input into OSCINP, and SPI CLK will be controlled at 24MHz.
It is required for system review (make sure the time from SPI CS#(39PIN) to Lock Detect(38PIN) is within 50us). Could you do an experiment for me?
Thank you
J.H. KIM