Part Number: LMK04828
Tool/software:
Hello,
We are going to use the LMK04828 fed by this really stable OXCO with the following output:
RF Output Signal Sinewave@ 100 MHz Load 50 Ohms
Output Power +9.0 +13.0 dBm 50 Ohm load
Harmonics -30 dBc 50 Ohm
load Spurious -80 dBc 50 Ohm load
We have been reading there are problem with the slew rate with sine wave input for clock reference. In the case of the output power we were thing of adding a 3 dB Pi attenuator to fit under the 2.4 Vpp of the LMK04828 input.
¿ Is this input compatible with the IC? ¿Do we have to take another consideration?
Thanks in advance for your help
Thanks in advance for your help.