Part Number: LMK61E2
Other Parts Discussed in Thread: USB2ANY,
Tool/software:
Hi, TI expert.
There is an inquiry from a my customer regarding LMK61E2.
[Question]
Although control was performed based on the datasheet, there is no change in clock output.
OSC is outputting 150MHz.
I will explain normal operation and N.G operation below, so please give me some advice.
1. Normal operation (OK)
- Read-only registers are read normally.
- The value written to the R/W Register is Rad.
2. N.G operation
- To change the frequency, D, INT, NUM, DEN, and OUTDIV values were described, but the output did not change at 150Mhz.

- I have set it up to write the SARM value to the EEPROM. (R49 , 0x40)
→ I have set the SARM value to be written to the EEPROM. (R56 , 0xBE) → (R49 , 0x1) , Wait for about 1s of delay between each command.
→ There is no change in EEPROM write Count (NVMCNT = 0x1).
→ When committing the EEPROM value to the register with (R49, 0x08), the register value changes but it is not the expected value.
Please give me advice regarding the N.G. operation described above.
Thanks.