Part Number: LMX2594
Tool/software:
Hello,
I am writing with an additional question about the LMX2594.
Currently, I need to output frequencies from 13.9GHz to 14.7GHz in 1kHz increments.
However, when I start at 13.9GHz and change to 13900.001, 13900.002, 13900.003MHz, at 13900.003MHz, I get outputs at 13900MHz, 13900.003MHz, and 13900.006MHz as shown in the attached image.

At 13900.004MHz, I get outputs at 13900MHz, 13900.004MHz, and 13900.008MHz.
This happens every time I move by 1kHz.
(In integer mode, there is no problem. ex : 13.9GHz)
I am using the following settings:
PFD: 100MHz
MOD: 1000000
Could you please explain why this issue is occurring?
Thank you.