LMX2594: PLL Question

Part Number: LMX2594

Tool/software:


Hello,

I am writing with an additional question about the LMX2594.

Currently, I need to output frequencies from 13.9GHz to 14.7GHz in 1kHz increments.

However, when I start at 13.9GHz and change to 13900.001, 13900.002, 13900.003MHz, at 13900.003MHz, I get outputs at 13900MHz, 13900.003MHz, and 13900.006MHz as shown in the attached image.


At 13900.004MHz, I get outputs at 13900MHz, 13900.004MHz, and 13900.008MHz.

This happens every time I move by 1kHz.

(In integer mode, there is no problem. ex : 13.9GHz)

I am using the following settings:

PFD: 100MHz
MOD: 1000000

Could you please explain why this issue is occurring?

Thank you.