Part Number: LMK04828BEVM
Other Parts Discussed in Thread: LMK04828, LMK04826
Tool/software:
hello,
Our current application is to synchronize all the input and output clocks of the LMK04828, and the phases are aligned after the sync signal is controlled;
Now there are 3 questions : 1. The input and output are not synchronized, and the phase difference is also not fixed (it will change after each power-on restart). 2. After the sync signal is controlled, the waveform can be seen to flicker on the oscilloscope, but there is no change. 3. Is there a timing requirement when configuring registers for SPI?
【Current configuration】