Other Parts Discussed in Thread: LMK04828, TRF3705EVM, DAC3484EVM, TICSPRO-SW, CODELOADER
I can get the desired output clock frequencies (i.e. 256MHz LVDS and the DACCLK ranging from 64MHz to 512MHz, 2x to 16x interpolation respectively) from the on-board 19.2MHz VXCO. Sooooo...I need to now input this frequency from the LMK04828BEVM whose input is a 10MHz reference clock. So I'm trying to generate a 19.2MHz LVPECL and 512MHz LVDS from a 10MHz input clock using the LMK04828BEVM. I'm having trouble setting this up using the Clock Design Tool as it defaults to the LMK04808B and won't select the LMK04828B. I can go in and select the LMK048028B using manual setup. The manual entyr method doesn't work for this device. Is there wizard tool that allows me to set up the LMK04828B for a 10MHz input generating both 19.2MHz and 512MHz outputs?