Part Number: LMK04828BEVM
Other Parts Discussed in Thread: LMK04828, LMK04821, LMK04806
Hello all
I am using LMK04828B Evaluation Board to generate some clocks using its internal oscillator which is Crystek-CVHD 950 100M in our board.
I am using TI Code Loader to program and configure the board. I need to get 60MHZ, 16MHz and 800KHz signal from this board and I was thinking of using SDCLKout for 800KHz signal and DCLKout0 and DCLKout1 for 60MHz and 16MHz signals. I could generate some signals following instruction posted by TI, but the frequency does not match the frequency predicted by software and I have seen changing some values in CLKout tab ( like PLL2 N and prescale N, or R) won’t affect the result at all. I really appreciate it if someone can help me out and let me know how I can setup the board correctly. Why changing some parameters will not impact the output at all.
Thanks