Other Parts Discussed in Thread: TPL5110
Tool/software:
Hi.
Many thks.
Is the following case possible? To use two pcs of TPL5010. Very economical and flexible component.
Remarks (schematic attached):
1) For watchdog timer use - can the WAKE signal be unconnected? No need in WDT use. The TPL5010 datasheet says "The DONE signal resets the counter of the watchdog only"
2) After POR Q3 is in OFF state - only U9 is "active" during Linux loading -100sec timeout.
3) When the app program starts, one DONE (WDI) pulse to confirm to reset counter of both TLP's.
4) Then set WDS to logic "1" - Q4 to ON state - U15 is "active" - 2sec timeout.
5) WDI pulse every second as normal WDT to both TPL's.
OK?
BR Jussi8688.TPL5010-1.pdf