This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCEL913: Clock generator programming

Part Number: CDCEL913

Tool/software:

Dear Expert,

In the previous discussion, it was advised to use a 20 MHz reference clock. As per the schematic, we are currently utilizing a 20 MHz crystal oscillator. Could you please clarify if additional configuration of the clock generator is required, or if it can remain in its default configuration?

Link to the previous discussion: TI E2E Forum - CDCEL913 Design Verification.

Thank you.
Adarsh Verma

  • Adarsh,

    Yes additional configuration of the clock generator is required as the device default expects a 27MHz input clock. The EEPROM can be programmed through I2C with the desired config. Once the EEPROM is programmed, then the device will power on with the new config and no additional register writing will be required. 

    Best,

    Cris