Tool/software:
Hi Experts, I have the LMK05318B on custom board and it works very well.
XO OCXO 24.576MHz
Ref1 GPS PPS
Ref2 IEEE1588 PPS optional
out1 25MHz
out2 10MHz
out7 PPS
When Ref1 is validated the output starts folowing. In one minute LOFL_DPLL goes low and after a while we have also DPLL phase lock, LOPL_DPLL low.
Tuning word history update HIST bit flashes periodic. R14 now is mostly 0x00 except for HIST bit.
I have adjusted the OCXO +0.1 PPM by purpose to see the difference between holdover and freerun.
But when i interrupt gps reception the LMK always falls to XO ppm offset instead of calculated averaged historical offset.
Expected the LMK holds the locked freq offset as long as no ref input in valid.
What am i doing wrong?
R185 0x00B9F5
R186 0x00BA01
R187 0x00BB00
R188 0x00BC00
R189 0x00BD00
R190 0x00BE00
R252 0x00FC2D
R0 0x000010 R1 0x00010B R2 0x000235 R3 0x000332 R4 0x000404 R5 0x00050E R6 0x000617 R7 0x00078E R8 0x000802 R10 0x000AC8 R11 0x000B00 R12 0x000C13 R13 0x000D08 R14 0x000E00 R15 0x000F00 R16 0x001000 R17 0x00111D R18 0x0012FF R19 0x001308 R20 0x001420 R21 0x001501 R22 0x001600 R23 0x001755 R24 0x001855 R25 0x001901 R26 0x001A00 R27 0x001B00 R28 0x001C01 R29 0x001D10 R30 0x001E40 R32 0x002044 R35 0x002300 R36 0x002403 R37 0x002500 R38 0x002600 R39 0x002702 R40 0x00280E R41 0x002900 R42 0x002A11 R43 0x002BC2 R44 0x002C00 R45 0x002D08 R46 0x002E88 R47 0x002F07 R48 0x003050 R49 0x00314A R50 0x00321C R51 0x003310 R52 0x003410 R53 0x003563 R54 0x003610 R55 0x003700 R56 0x0038F9 R57 0x003900 R58 0x003AF9 R59 0x003B00 R60 0x003C0F R61 0x003D00 R62 0x003E0F R63 0x003F3E R64 0x004095 R65 0x004102 R66 0x0042F8 R67 0x0043FF R68 0x004405 R69 0x004500 R70 0x004600 R71 0x004700 R72 0x004833 R73 0x004900 R74 0x004A00 R75 0x004B00 R76 0x004C00 R77 0x004D0F R78 0x004E00 R79 0x004F11 R80 0x005080 R81 0x00510A R82 0x005200 R83 0x00530E R84 0x005466 R85 0x005567 R86 0x005600 R87 0x00571E R88 0x005884 R89 0x005981 R90 0x005A00 R91 0x005B14 R92 0x005C00 R93 0x005D0E R94 0x005E66 R95 0x005F67 R96 0x006000 R97 0x00611E R98 0x006284 R99 0x006381 R100 0x006429 R101 0x006501 R102 0x006644 R103 0x00670F R104 0x00681F R105 0x006905 R106 0x006A00 R107 0x006B64 R108 0x006C00 R109 0x006D32 R110 0x006EDC R111 0x006FD5 R112 0x007055 R113 0x007155 R114 0x007255 R115 0x007303 R116 0x007401 R117 0x007500 R118 0x007600 R119 0x007700 R120 0x007800 R121 0x007900 R122 0x007A00 R123 0x007B28 R124 0x007C00 R125 0x007D11 R126 0x007E79 R127 0x007F7A R128 0x008000 R129 0x008101 R130 0x008200 R131 0x008301 R132 0x008401 R133 0x008577 R134 0x008601 R135 0x00871A R136 0x008880 R137 0x008900 R138 0x008A00 R139 0x008B03 R140 0x008C02 R141 0x008D00 R142 0x008E01 R143 0x008F01 R144 0x009077 R145 0x009101 R146 0x009289 R147 0x009320 R149 0x00950D R150 0x009600 R151 0x009701 R152 0x00980D R153 0x009929 R154 0x009A24 R155 0x009B32 R156 0x009C01 R157 0x009D00 R158 0x009E00 R159 0x009F00 R160 0x00A0FC R161 0x00A132 R162 0x00A200 R164 0x00A400 R165 0x00A500 R167 0x00A701 R178 0x00B200 R180 0x00B400 R181 0x00B500 R182 0x00B600 R183 0x00B700 R184 0x00B800 R185 0x00B9F5 R186 0x00BA01 R187 0x00BB00 R188 0x00BC00 R189 0x00BD00 R190 0x00BE00 R191 0x00BF00 R192 0x00C0D0 R193 0x00C118 R194 0x00C218 R195 0x00C300 R196 0x00C400 R197 0x00C51D R198 0x00C600 R199 0x00C700 R200 0x00C81D R201 0x00C900 R202 0x00CA00 R203 0x00CB00 R204 0x00CC15 R205 0x00CD00 R206 0x00CE00 R207 0x00CF15 R208 0x00D000 R209 0x00D114 R210 0x00D200 R211 0x00D316 R212 0x00D400 R213 0x00D514 R214 0x00D600 R215 0x00D716 R216 0x00D800 R217 0x00D900 R218 0x00DA00 R219 0x00DB19 R220 0x00DC6E R221 0x00DD00 R222 0x00DE03 R223 0x00DF0D R224 0x00E047 R225 0x00E100 R226 0x00E200 R227 0x00E319 R228 0x00E46E R229 0x00E500 R230 0x00E603 R231 0x00E70D R232 0x00E847 R233 0x00E910 R234 0x00EA10 R235 0x00EB02 R236 0x00ECEE R237 0x00ED00 R238 0x00EE00 R239 0x00EF02 R240 0x00F0EE R241 0x00F100 R242 0x00F200 R243 0x00F33F R244 0x00F43F R249 0x00F921 R250 0x00FA00 R251 0x00FB23 R252 0x00FC2D R253 0x00FD00 R254 0x00FE00 R255 0x00FF00 R256 0x010000 R257 0x010101 R258 0x010200 R259 0x010301 R260 0x010402 R261 0x010580 R262 0x010601 R263 0x01072A R264 0x010805 R265 0x0109F2 R266 0x010A00 R267 0x010BA0 R268 0x010C04 R269 0x010D00 R270 0x010E02 R271 0x010FB1 R272 0x011000 R273 0x011100 R274 0x011200 R275 0x011316 R276 0x011416 R277 0x011516 R278 0x011600 R279 0x011700 R280 0x011800 R281 0x011900 R282 0x011A00 R283 0x011B00 R284 0x011C1E R285 0x011D1E R286 0x011E00 R287 0x011F00 R288 0x012000 R289 0x012100 R290 0x012203 R291 0x012322 R292 0x012401 R293 0x012501 R294 0x012600 R295 0x012724 R296 0x01280A R297 0x01290A R298 0x012A0A R299 0x012B01 R300 0x012C00 R301 0x012D1C R302 0x012E1E R303 0x012F01 R304 0x01300F R305 0x013104 R306 0x013261 R307 0x0133F8 R308 0x013443 R309 0x0135C3 R310 0x0136C3 R311 0x0137C3 R312 0x0138C3 R313 0x0139C3 R314 0x013AFF R315 0x013BFF R316 0x013CFF R317 0x013DFF R318 0x013EFF R319 0x013F03 R320 0x014000 R321 0x01410A R322 0x014200 R323 0x014300 R324 0x014400 R325 0x014501 R326 0x014606 R327 0x014735 R328 0x014875 R329 0x01490B R330 0x014A00 R331 0x014B64 R332 0x014C00 R333 0x014D3D R334 0x014E09 R335 0x014F00 R336 0x015006 R337 0x015135 R338 0x015275 R339 0x01530B R340 0x015400 R341 0x015500 R342 0x015600 R343 0x015700 R344 0x015800 R345 0x015900 R346 0x015A03 R347 0x015B00 R348 0x015C00 R349 0x015D00 R350 0x015E00 R351 0x015F01 R352 0x016000 R357 0x016528 R367 0x016F00 R411 0x019B0C
Hi Octo,
Just to clarify, are you setting the OCXO to +0.1ppm during the whole duration of this test? If I'm understanding correctly on the output of the LMK05318B you're seeing:
Initial startup (LOFL = 1): +0.1 ppm
Around a minute later (LOFL = 0): 0 ppm (locked to 1pps input)
History accumulation: 0 ppm (locked to 1pps input)
1pps reference is lost (LOFL = 1): 0.1 ppm (holdover)
It looks like you have intermediate updates enabled so during holdover the device should automatically use the latest free run word. If intermediate updates were not enabled, you would generally need to wait for at least 3 Tavg periods plus the delay timer to ensure that the history is valid (see Figure 9-20 in the datasheet). Do you see any difference with different intermediate update intervals? I can also see if I can replicate this behavior on an EVM early next week.
Regards,
Connor
Indeed the OCXO +0.1ppm during the whole duration of this test and your description is correct. That's what i am seeing.
The intermediate updates enabled and also tested with different intervals. Same result.
Awaiting for the EVM test
Makes sense, thanks for the clarification. I'll go ahead and test this out on an EVM and see if I can replicate this behavior. I should be able to get back to you sometime tomorrow.
Regards,
Conor
thanks a lot so far.
In the meantime I am assembling another board to rule out a physical defect. You never know.
First time i brought up the LMK on my board, i initialized it with wrong values or random values, due to byte vs word i2c bus function. Had to wrote own programmer using HexRegisterValues output from Tics Pro. Power on reset and softreset didn't help.
After that i resetted all registers (R0 counting to R512) with zero and configured using HexRegisterValues file.
Is it possible that i overwrote some factory calibration or function routing/disablement?
Hi Octo,
My apologies for the delayed response, for some reason this thread had gotten marked as closed so I didn't see it was still ongoing. I wasn't able to replicate the error you described an an EVM. If you initialized the device with random values, it is possible that some trim settings got overwritten, but I think this would be unlikely to cause long term issues if you didn't program the EEPROM with an invalid config. Do you see the same behavior on the new board?
Regards,
Connor
Thank you for your response. I reworked the board with a new LMK chip so we can forget the eventually overwritten registers in eeprom.
Unfortunately it didn't help. Got again 1PPS, 10MHz and 25MHz output freq/phase locked in a few minutes to the GPS reference.
But after interrupting the antenna signal the LMK seems to not use the history but produces with OCXO's center frequency.
Hi Octo,
Jumping in here a bit...I noticed intermediate updates were discussed. Can you please try repeating the test with intermediate updates disabled? R185 (0xB9)= 0x05
Can you also please specify which history intermediate interval values you have tested?
Regards,
Jennifer