My BQ32000 circuit is as showed
I am using CR1220(35mAH) as back up battery for BQ32000.
When VCC is powered (+3.3V), BQ32000 is working fine.
During VCC powered off, the BQ32000 is powered by CR1220 battery, but the battery can only suport for
couple months(I guess 3 ~4 months), not all modules's battery is drained up, around 50% still working, 50% is drained up.
I measured Resistance between the BQ32000 BAT PIN(PIN3) to GND, the resistance is around 14MEG OHM.
Is there any need to configure BQ32000 register to lower the battery working current ?
or is there any sneak path from battery to GND ?
or probably the battery problem ?
Thanks !