Hi,
I am planning to use LMX2581 to provide clock to ADC12D1800, How to interface this two devices(Clock signal alone) . Since both the device supports differential clock signaling. What is the use of pullup resistors at the output pins ? whether is it must ? what will be the o/p power level if pullup resistors are not provided ?
Note: As per my application I want 3.1GHz sampling frequency & RFout channel B I planned to use it for another application with divide factor of two.
Regards,
Rajesh