This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As Windows XP is no longer supported, I am required to use a Windows 7 machine.
I need to program a CDCE706 via a parallel port.
I have installed a PCIe parallel port on the computer, but it is using non-standard addresses.
I have installed the Labview Run Time from:- "http://www. ni.com/download/labview-run-time-engine-8.2.1/550/en/", but this might not support Windows 7.
I have installed TIClockPro from scac097a, but this might not support Windows 7.
The TiClockPro GUI starts and allows me to set the address of the parallel port, but I cannot get the CDCE706 to program.
Has anyone managed to get TiClockPro working with a parallel port on Windows 7?
Do you know which part of my setup is not working, and how to fix it.
Thanks, for reading my query.
Mike.