This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
In one of my application I am looking for generation of Audio Clock frequency of 24.576MHz from Video clock. The Video Clock can be 27MHz to 148.5MHz. I would like to know if there any TI Clock & Timings devices suggested for this application.
Regards,
Ritesh
Thanks Julian. In case of CDCE913, I hope there will not be ppm errors in case of any of the input frequencies, 148.5MHz, 148.5MHz,/1.001, 74.25MHz, 74.25MHz,/1.001 and 27MHz.
Also I am looking for the following,
1. fixed clock multipliers x2, x4 with input clock frequency of 3.072MHz. Are these available in TI portfolio.
2. zero delay 1:2 buffers and a switch or clock mux for the Video clock. I need to route the video clock coming from 2 sources to CDCE913. So I am thinking of 1:2 zero delay clock buffer and a clock switch or Mux. Are these available in TI portfolio.
Regards,
Ritesh