This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Can you please help with the following customer questions
1. What is the current consumption?
Is it (Static supply current)+(supply current) = 45 + 177 = 222mA ?
2. What is the additive jitter that I need to consider?
Is it 0.3ps RMS (as mentioned is table in page 5 in datasheet)? Or is it 171fs RMS (as mentioned is table in page 6)?
3. What do I do with Vac_ref? what is its application?
Best regards,
Nir.