Other Parts Discussed in Thread: CDCE62005, LMK03318, CDCM6208
Dear Team,
Can you please help finding the most appropriate clocking device for the spec below ?
- Two LVDS-type inputs with hard-switch between them (by external PU/PD), with no need to prior programming of any kind.
- At least 4 outputs (no need for much more, exactly 4 is also OK), each to be able to support LVCMOS (3.3V) as well as differential (LVDS)
- Dividers on outputs (at least by 2)
- At least one output to start upon power up from the active input (with no need for programming)
Can the LMK03328 answer for the above ?
Can you advise alternative devices ?
Best Regards,
Nir