Other Parts Discussed in Thread: CDCE62005
Hi :
Need kind help on CDCE62005 design.
I use 10MHz reference clock for PRI_REF and SEC_REF, and use VC++ Interface code to set up registers, I tried many register configurations, one of the register setting is as below:
Reg_0 0xEB840000
Reg_1 0xEB840021
Reg_2 0xEB860302
Reg_3 0xEB860303
Reg_4 0xEB860334
Reg_5 0x800C6E45
Reg_6 0x84BE19C6
Reg_7 0xFD90FBA7
Reg_8 0x200099F8
After writing these registers, I can read back the same setting through sSPI_MISO on all registers, which tells me SPI interface is working.
The purpose of the design is to see two output clocks on U0 and U1 generated from PRI_REF input. But, I couldn't see clock signals on any output ports.
I don't know if it's hardware problem or not. Can anyone help me check the setting or give any suggestions?
Thank you very much in advance!