Other Parts Discussed in Thread: TLV1702
Hello,
Does the part tlc551 truly function down to 1V or am I missing something? For example, do the propagation delays from input to output become really slow?
Also, I'm trying to find out more about the CONT pin on part tlc551. The datasheet says that the CONT provides direct access to the 2/3 point on the voltage divider, and that BOTH the threshold voltage AND the trigger voltage are adjustable from the control pin. So the questions are:
1.) How close to Vdd can the CONT pin be(but still less than Vdd) while still maintaining functionality of the THRESH and TRIG pins? Likewise, how close to GND can the CONT pin be? Are we talking 50mV or so here?
2.) Relating to question 2: I'm assuming that more overdrive on the comparators implies faster overall switching. So then, would the comparator become very slow if CONT was brought close to either Vdd or GND?
3.) If, hypothetically, the CONT were tied to Vdd, then would the threshold value then become 1/2 Vdd since this would effectively short out the top resistor?
Thanks